Skip to main content
Tamas Novak
Associate III
Mar 18, 2017 11:30 PM UTC
Question

logic output max current for ST3232C

Posted on March 19, 2017 at 00:30

I'd drive an opto-isolator's LED directly from the logic output of ST3232CTR (VCC=5V). I'd set current with a serial resistor (Vcc - R - LED - 3232's output.  Output=L to light the LED up). 

I checked 'DocID7454 Rev 12' and found fig.5 and 6 with Uo=f(IoL) graph for VCC=5.5 and 3V.

As current is widely changes by the Vcc, I'm looking for a figure with multiple graphs for different supply voltages.

Can anyone help?

    This topic has been closed for replies.