Skip to main content
jiang jun
Visitor II
Dec 27, 2017 3:15 AM UTC
Question

LIN sensor problem

Posted on December 27, 2017 at 04:15

I have a Pepper+Fuchs sensor which interface is LIN(attachements are datasheet & user manual ). I need to test the sensor by computer so I purchased RS232 to LIN converter. I send 

handshake command on computer to the converter and it respone telegram correctly. The telegram format of converter is as below:

0690X00000609IsQAI.png

While 

telegram format of Pepper+Fuchs sensor is as below. When i send telegram following below to the sensor, there is no respone at all. Due to the 2 type telegram format is different , i don't know where is the problem. Is there anyone can help me?

0690X00000609IwQAI.png

#232-lin-converter
    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Jan 8, 2018 9:32 AM UTC
    Posted on January 08, 2018 at 10:32

    Hello ,

    this component is using 'Interface Interface type Physical LIN interface Transfer rate 19.2 kBit/s (8N1) Cycle time 100 ms'

    i do not think that it is a ST device.

    i recommend you to contact Pepper Fuchs community website

                   Best regards

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.