Skip to main content
ldong.1
Associate III
September 10, 2023
Question

L9369 getting voltage from SH1, SH2

Hello. ST team.

i'm using L9369's voltage measurement function.

i read L9369 manual, and i send below SPI commands(no.0~6) for initial driving.

(my purpose is to drive FET : HS1 A, B ON / LS2 A,B ON)

00xb5019ff8
10xb5a15fef
20xb720b54d
30xb480aa98
40x40a0000d
50xbb8020ea
60xc3a000f5

after sending above SPI commands to check SH1/2_A/B's voltage AD read.

140x0c20001f
150x0d000010
160x0e200001
170x0f00000e
180x1020001a
190x1620001d
200x17200012
210x1800000d
220x19200002
230x1a000013
240x11000015
250x12200004
260x1300000b
270x14200003
280x1500000c
290x1b00001c
300x1c200014
310x1d00001b
320x1e20000a
330x1f000005

after sending above SPI commands, i checked measured data, but the measured voltage is approximately 0.6V lower than the actual measurement value obtained through the oscilloscope.

After completing the above operation, I send the following SPI commands(no.7~13) again.

(my purpose is to drive FET : HS2 A, B ON / LS1 A,B ON)

70xb5019ff8
80xb5a0bfea
90xb7015548
100xb4a0aa98
110x4080000d
120xbba020ea
130xb401994d

After sending above SPI commands(no.14~33), i measure SH1/2_A/B's voltage again.

In the second operation, I confirmed that the values measured with the SH pin's AD value and those measured with the oscilloscope were nearly same.

My question is this: Why is the voltage output approximately 0.6V lower in the first operation? What SPI settings do I need to configure? (All four ACT_OFF_LS pins are in a low state after the first operation, switched to a high state to stop the H-bridge after the first operation, and then switched back to low just before the second operation to enable the H-bridge again.)

 

please let me know. thank you.

This topic has been closed for replies.

1 reply

ST Employee
September 14, 2023

Hi ldong.1,

 

This question has been routed to the online support center for direct support by our specialist team. Please check your account for updates and support regarding this request.

 

Regards,
Jake

ST Support