Skip to main content
July 14, 2026
Question

L6360 Master Not Receiving Response from L6364Q IO-Link Device

  • July 14, 2026
  • 0 replies
  • 56 views

Hello everyone,

I'm trying to establish communication between an IO-Link master and an IO-Link device, but I'm very new to this field and I'm having a lot of difficulty getting the communication done.

I'm using a STEVAL-IOM001V1 with the L6360 transceiver. I generate an 80 µs wake-up pulse on the bus using a timer in alternate function with the USART. Then, through my state machine, I'm able to send a Type_0 message with MC = 0xA2 and the corresponding checksum at different transmission rates, while keeping the Tdmt timing between consecutive messages within the required range of 27–37 Tbit.

Using an oscilloscope, I can see that the wake-up sequence (Twup + Tren) and the messages are correctly generated and transmitted to the device. However, in most cases, the device does not respond.

As the IO-Link device, I'm using an X-NUCLEO-IOD02A1 with the L6364Q transceiver and the ST example software with the MiniStack.

Has anyone experienced a similar issue or have any suggestions on what I might be missing?

Any advice would be appreciated. Thank you!