Skip to main content
T.Ratheesh
Associate II
Jan 21, 2016 12:31 PM UTC
Question

Issue in BlueNRG Scanning using STEVAL board in Central role

Posted on January 21, 2016 at 13:31

Hi,

        I have the following boards STEVAL-IDB002V1 & STEVAL-IDB003V1 USB dongle (Both supporting BlueNRG chip alone).

Out of these boards, 1 is configured as Peripheral role and another is configured to Central role with Mode 2 as default option.

When I do the scanning through the Central device, I am able to observe that only the peripheral device is getting listed even though there are other BT devices outside which also are peripheral devices.

If I scan through my mobile supporting BT BLE4.0 and above, all the devices including the STEVAL peripheral devices is getting detected.

1.Is it an expected behaviour of the ST EVAL board which is running in Central Mode?

2.Is there a possiblity to scan other devices too as performed in mobiles?

If required, I can send the screenshots of the scanned device lists?

Could someone help me out in this regards as I am very new to this work?

Regards,

Ratheesh
This topic has been closed for replies.

1 reply

Scott Löhr
Senior III
Apr 18, 2017 8:11 PM UTC
Posted on April 18, 2017 at 22:11

Are you using a sample app from ST, or is this all your own embedded code that you are running?