Skip to main content
Jackie1
Visitor II
Aug 30, 2018 1:39 PM UTC
Question

Is there a programming guide doc for STUSB1702? For instance, I want to know how to make use of the BMC feature and how to set the voltage levels for power advertisements. Also, how do I advertise I_BUS > 3A?

..

    This topic has been closed for replies.

    1 reply

    Gregory Go.
    Senior III
    Sep 4, 2018 10:19 PM UTC

    Hi,

    The STUSB1702 is a USB-PD controller for Power Source applications (Provider), and with Automotive grade support (AEC-Q100 qualified).

    The STUSB1702 is supported with SPC5x family of MCUs, because SPC5 is automotive grade.

    https://www.st.com/en/automotive-microcontrollers/spc5-32-bit-automotive-mcus.html

    There is no programming guide available. But there are programming examples in the X-CUBE-USB-PD software library.

    https://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-usb-pd.html

    If you don't need the Automotive grade in your application, it is recommended to use the STUSB1602 instead of STUSB1702.

    The STUSB1602 is supported with STM32 Microcontroller family.

    The examples for USB-PD Provider are located in the X-CUBE-USB-PD package here:

    • STM32CubeExpansion_USBPD_F0_V2.1.0\Projects\STM32F072RB-Nucleo\Applications\USB_PD\MB1303_Provider_RTOS

    • STM32CubeExpansion_USBPD_F0_V2.1.0\Projects\STM32F072RB-Nucleo\Applications\USB_PD\MB1303_Provider_PD30