Skip to main content
nono3139
Visitor II
Apr 26, 2019 12:46 PM UTC
Question

Is the S2-LP based nucleo shield only 868Mhz and not 433MHz ?

I want to use an S2-LP based nucleo shield to communicate in FSK with a 433MHz device.

I bought the X-NUCLEO-S2868A1 and then noticed that the shield seems tunes only for 868MHz.

I do not seem to find on the ST website a reference for a corresponding board tuned for 433MHz. Is there a reason ?

I can see the eval kit STEVAL-FKI433V2 that seems to contain a shield tuned for 433MHz but the shield itself does not seem to be available anywhere (no actual reference)

    This topic has been closed for replies.