Skip to main content
Egemen
Associate II
Mar 16, 2023 9:01 AM UTC
Solved

Is positive and negative pins matter for ECMF4-40A100N10

Can we connect D1+ to DN and D1- to DP (same for the connector (D1+CON to USB_D_N))

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Mar 16, 2023 10:01 AM UTC

    The common mode filter is symmetrical in itself. The pin assignment with + and - is primarily there to have the assignment to the same pin on the connector and on the IC.

    As long as you make sure that the correct filter is used (D1 for port 1, D2 for port 2) and DN and DP end up "through the inductance" at the correct pin of the IC, everything is OK.

    Does it answer your question?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    1 reply

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Mar 16, 2023 10:01 AM UTC

    The common mode filter is symmetrical in itself. The pin assignment with + and - is primarily there to have the assignment to the same pin on the connector and on the IC.

    As long as you make sure that the correct filter is used (D1 for port 1, D2 for port 2) and DN and DP end up "through the inductance" at the correct pin of the IC, everything is OK.

    Does it answer your question?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.