Skip to main content
Skada.3
Associate III
Jun 11, 2019 11:19 AM UTC
Question

Is it possible to update firmware by OTA using mobile app for spbtle-1s ?

I am newbie of ST controller.

I am working with STEVAL-BLUEMIC-1. this module contains spbtle-1s which is based on BlueNRG-1. According to the application note AN4869, firmware can update using another BlueNRG-1as central.

But I want to update firmware using mobile app. Is it possible and how?

    This topic has been closed for replies.

    5 replies

    Winfred LU
    ST Employee
    Jun 13, 2019 1:52 AM UTC

    Please try BlueDFU v1.0.10:

    Android: https://play.google.com/store/apps/details?id=com.st.STBlueDFU

    iOS: https://itunes.apple.com/it/app/st-bluedfu/id1187882971

    It is tested working with STEVAL-IDB007v2 (BlueNRG-1), DK 3.1.0.

    Skada.3
    Skada.3Author
    Associate III
    Jun 13, 2019 4:57 AM UTC

    Hi Winfred LU

    Thanks for the answer.

    Along with android side I need help on Embedded side. In STEVAL-BLUEMIC-1 firmware files I am not getting any OTA service. So can I use the same service mentioned in the application note as I mentioned before or any other service is required?

    Winfred LU
    ST Employee
    Jun 14, 2019 5:23 AM UTC

    Hi Suvarna,

    Yes. Actually the same OTA service is required.

    Please refer to AN4869 - The BlueNRG-1, BlueNRG-2 BLE OTA (over-the-air) firmware upgrade :

    https://www.st.com/resource/en/application_note/dm00293821.pdf

    Section 2.2.2, BLE application with BLE OTA service

    and modify the firmware (application) accordingly. 

    Best Regards,

    Winfred

    Skada.3
    Skada.3Author
    Associate III
    Jul 3, 2019 9:40 AM UTC

    hi

    I am developing firmware for the OTA feature using steval-blumic-1 project folder.

    In file 'OTA_btl.c' file I am getting following error

    error: #5: cannot open source input file "SDK_EVAL_Config.h": No such file or directory

    Where will I get this file for STEVAL-BLUEMIC-1 module?