Skip to main content
GTolk.1
Associate II
Oct 22, 2020 6:59 AM UTC
Question

Is it possible to set up IO-Link communication with the L6362 and use High-side or Low-side stage?

Hello everyone. 

I was wondering whether it is possible to set up IO-Link communication with the L6362 transceiver and not work in push-pull mode but in high-side-output stage or low-side-output stage mode? According to the data sheet, HS and LS can also be used when OUTH and OUTL are connected, but it does not state whether IOLink can still be used. Does anyone know if it's possible to use IOLink in HS or LS mode?

Datasheet L6362: https://www.st.com/resource/en/datasheet/l6362a.pdf

    This topic has been closed for replies.