Skip to main content
k_ovchinnikov
Associate
Nov 17, 2016 4:38 PM UTC
Question

Invalid HTTPD_FS image

Posted on November 17, 2016 at 17:38

Try to upload a new file to SPWF01S but have received subject error message. Why this file can't pass validation?

    This topic has been closed for replies.

    11 replies

    Gerardo GALLUCCI
    ST Employee
    Nov 18, 2016 8:53 AM UTC
    Posted on November 18, 2016 at 09:53

    Hi,

    which FW versione are you using?

    That error means that FS image is not sane. Header is not good. Did you use proper tool to create that image?

    To understand what's happening, can you please try to:

    - use HTTPDFSWRITE command (update via UART. Do not forget to enable flow control)

    - use again HTTPDFSUPDATE command, but with a different webserver

    This way we can understand if file is sane (and download was not good), or if file is not sane.

    Thanks

    jerry

    k_ovchinnikov
    Associate
    Nov 18, 2016 2:42 PM UTC
    Posted on November 18, 2016 at 15:42

    Hello. I'm using (150410-c2e37a3-SPWF01S) module.

    I create this image with gen.bat placed in stsw-idw002.rar downloaded from st.com

    There are no HTTPDFSWRITE command description in documents whitch I use (UM1695 User manual. Command set reference guide for ''AT full stack'' for SPWF01Sx series of Wi-Fi modules). So I don't know how to apply correct this command.  

    Gerardo GALLUCCI
    ST Employee
    Nov 18, 2016 2:54 PM UTC
    Posted on November 18, 2016 at 15:54

    Hi,

    that new command has been added to FW3.5.

    Please update to latest FW release,

    j

    k_ovchinnikov
    Associate
    Nov 18, 2016 3:41 PM UTC
    Posted on November 18, 2016 at 16:41

    Could you please point me to where I can get latest firm ware and documentation for newest command set.

    Gerardo GALLUCCI
    ST Employee
    Nov 18, 2016 4:38 PM UTC
    Posted on November 18, 2016 at 17:38

    STSW-WIFI001

    For *.11 modules (with embedded 1Mb flash)

    http://www.st.com/content/st_com/en/products/wireless-connectivity/wi-fi/spwf01sa.html

    k_ovchinnikov
    Associate
    Nov 21, 2016 3:45 PM UTC
    Posted on November 21, 2016 at 16:45

    Thank you for help. I downloaded file via UART.

    And now want to write script like output.cgi for receiving data from HTML form via UART. Where can I read about how to write script in relation to the module?

    Gerardo GALLUCCI
    ST Employee
    Nov 21, 2016 4:24 PM UTC
    Posted on November 21, 2016 at 17:24

    Cannot write script inside the webserver. All you can do is using what already existing: built-in scripts and SSI mechanism. Please take a look at AN4902

    : SPWF01Sx – dynamic web pages (http://www.st.com/content/st_com/en/products/wireless-connectivity/wi-fi/spwf01sa.html)

    Regards

    jerry

    k_ovchinnikov
    Associate
    Jun 15, 2017 6:44 PM UTC
    Posted on June 15, 2017 at 18:44

    Hello. I used html code from '

    SPWF01Sx – dynamic web pages' Output demo – multiple text boxes with script which allows skipping the automatic redirect. But after pressing submit button it redirect to output_demo.html. Why?

    Gerardo GALLUCCI
    ST Employee
    Jun 16, 2017 1:16 AM UTC
    Posted on June 16, 2017 at 01:16

    Because it's built on top of HTTP GET request. Request for some html resource. Which one? That one.