Skip to main content
Associate
September 25, 2024
Question

Interface the IW612 NXP module(LBES5PL2EL-923) with the STM32 MCU

  • September 25, 2024
  • 2 replies
  • 872 views
Hi,
 
We want to interface the IW612 NXP module(LBES5PL2EL-923) with the STM32 MCU and use it to communicate with Wi-Fi and BLE. 
 
We want to use the STM32 host to communicate with both BLE and Wi-Fi.
Does the STM32 provide any specific drivers to communicate with the IW612 BLE & WIFI?
For BLE, which uses a UART host interface, do we need any AT commands from the host side, or is another commands used?
Similarly, for Wi-Fi, which uses an SDIO host interface, do we need any AT commands from the host side, or is another commands used?
 
This topic has been closed for replies.

2 replies

Andrew Neil
Super User
September 25, 2024

@chiragTeksun123 wrote:
We want to use the STM32 host to communicate with both BLE and Wi-Fi.

Remember that the NXP device neither knows nor cares what microcontroller you use - you just have to follow whatever is defined in its interface documentation.

 


@chiragTeksun123 wrote:
Does the STM32 provide any specific drivers to communicate with the IW612 BLE & WIFI?

No - you would need to look to NXP for that kind of thing.

Most likely, they will provide "generic" drivers which just need you to provide a couple of specific host-specific interface functions.

 


@chiragTeksun123 wrote:
For BLE, which uses a UART host interface, do we need any AT commands from the host side, or is another commands used?

That's entirely down to the NXP device - the Host just needs to do whatever the NXP thing requires

 


@chiragTeksun123 wrote:
Similarly, for Wi-Fi, which uses an SDIO host interface, do we need any AT commands from the host side, or is another commands used?

Again, that's entirely down to the NXP device.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
September 25, 2024

@Andrew Neil wrote:
you would need to look to NXP for that kind of thing.

Looks like the module is actually from Murata:

https://www.murata.com/en-eu/products/connectivitymodule/wi-fi-bluetooth/overview/lineup/type2el#software

So also check out their documentation & support...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.