Skip to main content
Robert Kwan
Associate II
Apr 26, 2017 5:24 AM UTC
Question

IDW01M1 Wifi Sample Codes for STM32F411RE

Posted on April 26, 2017 at 07:24

Hello!

I recently bought the IDW01M1 WiFi expansion board 

and I am trying to have it working with the STM32F411RE.

However, from the examples in en.x-cube-wifi1_firmware.zip,

I can find the .bin file for STM32F401RE-Nucleo only

and so I tried to flash this WiFi_VCOM .bin to the STM32F411RE board.

I can see LED1 is green, so power is ok.

No other LED On, so module is ok?!

When I use Tera Term, I don't see any output and when I send 'AT', no 'OK' either.

So my question is that  F401RE .bin image cannot work directly on F411RE board please?!

Since I am still a newbie to this WiFi module, I am not sure if it will be easy to recompile the sample application for F411RE then?!

Any suggestion / comment is welcome.

Thanks & Best Regards,

Robert

#stm32f411re-wifi-idw01m1
This topic has been closed for replies.

41 replies

Robert Kwan
Associate II
May 31, 2017 9:51 AM UTC
Posted on May 31, 2017 at 11:51

Hi Mridu,

And I set more breakpoints to see when the ring buffer got to have the elements filled in

and I found that it's only when the program is running into the wifi_reset() but it would not come out of the wifi_reset() because it is trapped in the while() loop inside the wifi_reset().

Hope that you will have better idea on where to debug next...

Thanks & Best Regards,

Robert

Mridupawan Das
Visitor II
May 31, 2017 2:35 PM UTC
Posted on May 31, 2017 at 14:35

Check if you have WIND:32 on the ring_buffer.

If yes, check if you hit the :

1. void Process_Wind_Indication(uint8_t *process_buff_ptr) in file wifi_module_uart_01.c

2. void Process_DeQed_Wind_Indication(wifi_event_TypeDef * L_DeQued_wifi_event) in file wifi_module.c

    case WiFi_Hardware_Started :

in both functions above.

You should hit 1. If not then soemthing strnage is happening. So will have to investigate this first.

Then you should hit 2. If not , check if timer is running. Else further investigate on this.

Robert Kwan
Associate II
May 31, 2017 3:19 PM UTC
Posted on May 31, 2017 at 17:19

Hi Mridu,

I set breakpoint inside the beginning of 1. Process_Wind_Indication(uint8_t *process_buff_ptr) in file wifi_module_uart_01.c

and it doesn't get hit at all.

Then, so is 2.!

So what strange point are you thinking of please?

Thanks & Best Regards,

Robert

Robert Kwan
Associate II
May 31, 2017 3:21 PM UTC
Posted on May 31, 2017 at 17:21

And I checked the .map file ok with these 2 functions:-

 .text.Process_Wind_Indication

                0x08004f34      0x324 Middlewares/ST/STM32_SPWF0xSy/wifi_module_uart_01.o

                0x08004f34                Process_Wind_Indication

.text.Process_DeQed_Wind_Indication

                0x08004564      0x284 Middlewares/ST/STM32_SPWF0xSy/wifi_module.o

                0x08004564                Process_DeQed_Wind_Indication

Thanks & BR,

Robert

Robert Kwan
Associate II
May 31, 2017 3:29 PM UTC
Posted on May 31, 2017 at 17:29

Surprisingly, if I set the breakpoints to one level higher of these 2 functions where they would be called,

1. Process_Buffer() would not be triggered with the breakpoint for Process_Wind_Indication()

2. Wifi_TIM_Handler() would be triggered even though the Process_DeQed_Wind_Indication() would not be triggered.

So it seems that timer itself may be ok but not the Process_Buffer()?!

Thanks & Best Regards,

Robert

Robert Kwan
Associate II
May 31, 2017 3:36 PM UTC
Posted on May 31, 2017 at 17:36

It seems that Wifi_SysTick_Isr() cannot be triggered and then so Process_Wifi() and then so Process_Buffer()

but I don't know why Wifi_SysTick_Isr() cannot be triggered though...

Thanks & BR,

Robert

Robert Kwan
Associate II
May 31, 2017 3:51 PM UTC
Posted on May 31, 2017 at 17:51

Looking a bit deeper, I found that it's related to the SysTick_Handler() in the startup_stm32f411xe.s of sample codes

but I am using the mbed one which would be generated differently as startup_stm32f411xe.o in the mbed folder.

And this startup_stm32f411xe.o would not cover the SysTick_Handler() at all!!

Not sure if I can replace this one from mbed one or not?!

Any idea please?

Thanks & BR,

Robert

Robert Kwan
Associate II
Jun 1, 2017 11:26 AM UTC
Posted on June 01, 2017 at 13:26

Hi Mridu,

I tried different combinations of mbed files and the original Server_Socket files

but without much success.

1. In my previous builds, I didn't use the syscalls.c from Server_Socket sample but retarget.c from mbed.

    However, if I tried to use ./Projects/Multi/Applications/Server_Socket/SW4STM32/STM32F411RE-Nucleo/syscalls.o

    I would not be able to compile at all, so I have to stay with

    $(MBED_PATH)/$(TARGET_BOARD)/TOOLCHAIN_GCC_ARM/retarget.o 

  

So in my Makefile, I use all the other files from the Server_Socket sample except the syscalls.c:-

./Drivers/BSP/STM32F4xx-Nucleo/stm32f4xx_nucleo.o \

./Drivers/BSP/X-NUCLEO-IDW0xx1/stm32_spwf_wifi.o \

./Middlewares/ST/STM32_SPWF0xSy/Utils/event_buffer.o \

./Middlewares/ST/STM32_SPWF0xSy/Utils/ring_buffer.o \

./Middlewares/ST/STM32_SPWF0xSy/Utils/spwf04WiFi.o \

./Middlewares/ST/STM32_SPWF0xSy/Utils/wifi_globals.o \

./Middlewares/ST/STM32_SPWF0xSy/wifi_interface.o \

./Middlewares/ST/STM32_SPWF0xSy/wifi_module.o \

./Middlewares/ST/STM32_SPWF0xSy/wifi_module_spi.o \

./Middlewares/ST/STM32_SPWF0xSy/wifi_module_uart_01.o \

./Middlewares/ST/STM32_SPWF0xSy/wifi_module_uart_04.o \

./Projects/Multi/Applications/Server_Socket/Src/stm32_xx_hal_msp.o \

./Projects/Multi/Applications/Server_Socket/Src/stm32_xx_it.o \

./Projects/Multi/Applications/Server_Socket/Src/console.o \

./Projects/Multi/Applications/Server_Socket/Src/system_stm32f4xx.o \

./Projects/Multi/Applications/Server_Socket/SW4STM32/STM32F411RE-Nucleo/startup_stm32f411xe.o

##./Projects/Multi/Applications/Server_Socket/SW4STM32/STM32F411RE-Nucleo/syscalls.o

2. My latest build would not trigger the Wifi_TIM_Handler() as I reported yesterday after all the different trials.

    Since I didn't really modify any C codes, the only things I played around were the Makefile and the LinkerScript.ld.

    So I suspect that I made some wrong change in the LinkerScript.ld?!

    In fact, I use the one from mbed as the base:-

    LINKER_SCRIPT = $(MBED_PATH)/$(TARGET_BOARD)/TOOLCHAIN_GCC_ARM/$(TARGET_LD).ld

    and so some potential conflict with the files from Server_Socket sample?!

Therefore, I am clueless now...

Thanks & Best Regards,

Robert

Robert Kwan
Associate II
Jun 3, 2017 11:45 AM UTC
Posted on June 03, 2017 at 13:45

Hello!

I would like to ask if the SysTick_Handler in the isr_vector never gets triggered in my program,

how can I see if the interrupt flag is enabled correctly or not under Eclipse IDE / OpenOCD debug environment please?

Thanks & Best Regards,

Robert

Gerardo GALLUCCI
ST Employee
Jun 6, 2017 8:35 PM UTC
Posted on June 06, 2017 at 20:35

Hi,

you can check STM32 or Cortex-M4 reference manual to find the flag address. Probably it's a 0xE000something...

BR

j

Robert Kwan
Associate II
Jun 6, 2017 9:38 PM UTC
Posted on June 06, 2017 at 23:38

Thanks Jerry!

I found from the Cortex-M4 reference manual that

0xE000E010 STCSR SysTick Control and Status Register

0xE000E014 STRVR SysTick Reload Value Register

For the pure Socket Server sample app,

these two registers would have the values:-

0xE000E010 STCSR SysTick Control and Status Register  0x07000100

0xE000E014 STRVR SysTick Reload Value Register          0x1F480100

after wifi_init()

However, for my mixed mbed build,

I will have 0x0 only.

However, when I forced these two registers to have the same values,

0xE000E010 STCSR SysTick Control and Status Register  would take only 0x07000000

and the initialization will then be completed ok with the printf().

And SysTick Control and Status Register  would become 0x07000100 eventually as well.

Therefore, it seems that somehow my mixed mbed HAL drivers or the linkerScript.ld will make the SysTick initialization failed?!

However, I have no idea on how to debug this further.

Any suggestion please?

Thanks & Best Regards,

Robert

Robert Kwan
Associate II
Jun 7, 2017 12:05 AM UTC
Posted on June 07, 2017 at 02:05

Hello!

I observed another weird behavior when I tried to find out when the SYSTICK CTRL register would be set.

In the original Server Socket sample app,

I can step into the HAL_InitTick() and then I will go to the HAL_SYSTICK_Config() inside the core_cm4.h.

However, in my mixed build,

it would not get into any HAL_SYSTICK_Config() when I tried to step into the HAL_InitTick()

and similar problem to the following HAL_MspInit() too.

But when I checked the .map file, I can see:

.text.HAL_SYSTICK_Config

                0x00000000       0x38 c:/BG1/IoT/SensorTool_012017/RadioSensorlib/Matlab/Nucleo/mbed/TARGET_NUCLEO_F411RE/TOOLCHAIN_GCC_ARM/stm32f4xx_hal_cortex.o

while in the .map file of the original sample app:-

.text.HAL_SYSTICK_Config

                0x080004f4       0x2c Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal_cortex.o

                0x080004f4                HAL_SYSTICK_Config

So it seems that the mbed's stem32f4xx_hal_cortex.o is different from the sample app's...?!

Thanks & BR,

Robert