Skip to main content
Patrick Brennand
Associate
Nov 14, 2017 10:51 PM UTC
Question

IDB007V1 debug with STLINK

Posted on November 14, 2017 at 23:51

 

 

 

Hi

I am trying to debug with the IDB007V1 dvelopment board and a STLINK V2 but the debug process fails at the FLASH download.

I have tried the sensor and hello world demonstration programs with the same result.

0690X0000060MtpQAE_22955.png

Any help to start debugging would be appreciated!

Patrick

 

#bluenrg-1 #steval-idb007v1

This topic has been closed for replies.

7 replies

Andrea Palmieri
ST Employee
Nov 15, 2017 10:14 AM UTC
Posted on November 15, 2017 at 11:14

Hi Patrick,

please refer to

http://www.st.com/en/embedded-software/stsw-bnrg1stlink.html

.

Kind regards

Andrea

Patrick Brennand
Associate
Nov 16, 2017 12:48 AM UTC
Posted on November 16, 2017 at 00:48

Hi,

I want to run debug, not just program. How do I do that?

Thanks

Patrick

Andrea Palmieri
ST Employee
Nov 16, 2017 10:14 AM UTC
Posted on November 16, 2017 at 11:14

Hi Patrick,

could you use an alternative as toolchain? For example IAR Embedded Workbench which has also a 30 days free trial option?

Regards

Andrea

Frederic Germain
Visitor II
Nov 21, 2017 9:41 AM UTC
Posted on November 21, 2017 at 10:41

I had this problem too with latest version of TrueStudio.

I just ended up using another solution for build and flash...

So there is no easy way, for now, to evaluate these modules for beginners.

benjamin reynaud
Visitor II
Feb 28, 2018 9:59 AM UTC
Posted on February 28, 2018 at 09:59

Frederic,

Can you explain the procedure you applied to be able to work on this EVAL board ?

For what I saw, the Atollic toolchain could be the cause, the Keil one is OK but limited in its trial version.

BR

Frederic Germain
Visitor II
Jun 6, 2018 7:50 AM UTC
Posted on June 06, 2018 at 07:50

Sorry, haven't seen the notification until I login again.

I had a solution working with STEVAL-BLUEMIC-1.

I don't remember exactly, but it was probably a command line based solution, with some raw gcc + openocd.

I could try to find it again if you're interested again.

BlueNRG is a beautiful IC. So bad development support and bt stack is not up to it yet...

Vladislav Yurov
Associate III
Jun 11, 2018 2:04 PM UTC
Posted on June 11, 2018 at 16:04

Hi, you can debug in 'Eclipse like IDEs' after you properly configure your project settings. In original eclipse I'm able to debug with ARM MCU plugin for Eclipse and using OpenOCD.exe compiled by ST + use configurations file for openocd also from ST... You can find everything in 'BlueNRG-1_2 DK 2.6.0'.