Skip to main content
BV.1
Visitor II
Feb 12, 2020 11:59 AM UTC
Solved

I would like to develop a piconet using STM32 BluenRG 2 DK by setting up one master device and multiple slave devices. Every slave is connected to an analog sensor and the master should discover the slave, connect and receive data and disconnect.

STEMEVALIDB008 V2 is the board I am planning to use.

Link: https://www.st.com/en/evaluation-tools/steval-idb008v2.html

This topic has been closed for replies.
Winfred LU
Winfred LUBest answer
ST Employee
Feb 20, 2020 6:41 AM UTC

Please reference the documents in DK:

C:\Program Files (x86)\STMicroelectronics\BlueNRG-1_2 DK 3.1.0\Docs\Multiple_Connection_Guidelines\Multiple_Connection_Guidelines.html

C:\Program Files (x86)\STMicroelectronics\BlueNRG-1_2 DK 3.1.0\Docs\Multiple_Connection_Formula\Multiple_Connections_Formula.html

1 reply

Winfred LU
Winfred LUBest answer
ST Employee
Feb 20, 2020 6:41 AM UTC

Please reference the documents in DK:

C:\Program Files (x86)\STMicroelectronics\BlueNRG-1_2 DK 3.1.0\Docs\Multiple_Connection_Guidelines\Multiple_Connection_Guidelines.html

C:\Program Files (x86)\STMicroelectronics\BlueNRG-1_2 DK 3.1.0\Docs\Multiple_Connection_Formula\Multiple_Connections_Formula.html