Skip to main content
aoz.1
Associate
Apr 28, 2021 7:35 PM UTC
Question

I want to use hyperflash

I want to use hyperflash (S26KS512 or S26KL512) with stm32h723zet6 microcontroller.

The memory has "Phase Shifted Clock" pins.

What should I do with them? Connect to GND or VCC or Not Connected?

Hyperbus interface (stm32) support 1.8v?

    This topic has been closed for replies.

    2 replies

    aoz.1
    aoz.1Author
    Associate
    Jun 2, 2021 4:50 AM UTC

    Should I use a 1.8 volt power supply (VDD 1.8V)?

    Can I use 3.3 volt(VDD 3.3V) power supply with 1.8v hyperbus?

    Tesla DeLorean
    Guru
    Jun 2, 2021 6:50 AM UTC

    Seems like entirely the wrong subforum to post this.

    The KL model looks to be the 2.7 - 3.6V part, I certainly wouldn't be using the 1.8V part at voltages exceeding the maximums specified.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..