Skip to main content
SKuma.15
Associate
Jun 26, 2020 3:04 PM UTC
Question

I interface stm32H743Zi2 nucleo board with LDC1614. clock freq is varies.

SCL mode is Fast Mode but i.e whoes speed is 400KHz. but when i see in logic analyzer its shows 350-360KHz. Why its fluctute .

    This topic has been closed for replies.

    3 replies

    berendi
    Principal
    Jun 27, 2020 6:45 AM UTC

    Two possible reasons:

    The clock rate is too fast for the peripheral, and it is using clock stretching to slow it down. Check its datasheet to see whether it is supposed to do that.

    System clock setup code is broken in certain STM32CubeMX and HAL versions. There are various analyses and workarounds suggested in the forum, I have ended up writing my replacement according to the documentation in the reference manual. The failure mode was similar in my case, a clock which was supposed to be 100 MHz sometimes dropped to 90 MHz. Check the SystemInit() function as well, it too might be broken in later versions.

    SKuma.15
    SKuma.15Author
    Associate
    Jun 27, 2020 7:00 AM UTC
    According to the datasheet of ldc1614 . Clock stretching is not supported
    berendi
    Principal
    Jun 27, 2020 7:23 AM UTC

    Then it is time to get familiar with the RCC chapter of the reference manual.