Skip to main content
IShug
Associate
Aug 12, 2019 7:35 PM UTC
Question

I am trying to replicate SDK_BasicGeneric_A example transmitter code on my custom board. And it works well only after I set BYPASS_LDO to 1. What is the reason of such behavior?

Processor is PIC16LF18446, interface with s2lp works fine. I use S2LP_Library from SDK 1.2.1 with some adaptations for PIC. Three boards with the same behavior - possibility of soldering error is minimal. Frequency 433 MHz, crystal 50 MHz.

    This topic has been closed for replies.

    1 reply

    IShug
    IShugAuthor
    Associate
    Aug 17, 2019 5:25 PM UTC

    The reason was the malfunction of LDO regulators due to excessive capacitance of decoupling capacitor for band-gap voltage reference of VCO regulator. Changing this capacitance from 0.1uF to 390pF have fixed the problem.