Skip to main content
DPlay.1
Visitor II
Jul 14, 2020 10:45 PM UTC
Question

How to properly install firmware for for MKI109 with MKI197 sensor for mac

1) Having issue communicating with the board. After some googling, some post suggested that the firmware needs to be updated.

2A) Attempted to update firmware -- From reading the document, below command was used, but it failed due to the error in red below:

 $ dfu-util -a 0 -D /Users/chalinlee/Downloads/MEMS_Demonstration_Kit_SW_package_v9_8_MACOSX/FIRMWARE/ProfiMEMSTool\ board/ProfiMEMSToolV3.6.36.dfu -d 0483:df11

dfu-util 0.9

Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.

Copyright 2010-2016 Tormod Volden and Stefan Schmidt

This program is Free Software and has ABSOLUTELY NO WARRANTY

Please report bugs to http://sourceforge.net/p/dfu-util/tickets/

Opening DFU capable USB device...

ID 0483:df11

Run-time device DFU version 011a

Claiming USB DFU Interface...

Setting Alternate Setting #0 ...

Determining device status: state = dfuERROR, status = 10

dfuERROR, clearing status

Determining device status: state = dfuIDLE, status = 0

dfuIDLE, continuing

DFU mode device DFU version 011a

Device returned transfer size 2048

dfu-util: Error: File ID 0483:0000 does not match device (0483:df11 or 0483:df11)

2B) Attempted to update firmware -- by changing the device vendor product in green below with the following command and the upgrade seems to go through:

 $ dfu-util -a 0 -D /Users/chalinlee/Downloads/MEMS_Demonstration_Kit_SW_package_v9_8_MACOSX/FIRMWARE/ProfiMEMSTool\ board/ProfiMEMSToolV3.6.36.dfu -d 0483:0000

dfu-util 0.9

Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.

Copyright 2010-2016 Tormod Volden and Stefan Schmidt

This program is Free Software and has ABSOLUTELY NO WARRANTY

Please report bugs to http://sourceforge.net/p/dfu-util/tickets/

Opening DFU capable USB device...

ID 0483:df11

Run-time device DFU version 011a

Claiming USB DFU Interface...

Setting Alternate Setting #0 ...

Determining device status: state = dfuIDLE, status = 0

dfuIDLE, continuing

DFU mode device DFU version 011a

Device returned transfer size 2048

DfuSe interface name: "Internal Flash "

file contains 1 DFU images

parsing DFU image 1

image for alternate setting 0, (1 elements, total size = 292888)

parsing element 1, address = 0x08000000, size = 292880

Download [=========================] 100%   292880 bytes

Download done.

done parsing DfuSe file

3) Launch unico, but encountered adapter board detection issue with 'WHO_AM_I register' error below. It appears someone encounter similar issue in the past:

https://community.st.com/s/question/0D50X0000BVnrov/stswmki109w-firmware-upgrade

This topic has been closed for replies.