Skip to main content
OGaie
Associate II
Mar 20, 2020 12:03 PM UTC
Question

How to Interface ATWINC1500 xplained pro with STM32l46A6ZG Nucelo ?

Hey,

So i'm using the STM32l4A6ZG and and I want to implement the ATWINC1500 xpro driver so i can use the APIs to successfully connect the ATWINC1500xpro module to the STM32 Host MCU.

Can I use this driver :

https://github.com/gd91/stm32_winc1500_station_example

and change the includes from stm32f4xx to stm32l4xx ?

in that case which changes do I have to take and where to copy the following files.

Thank you,

This topic has been closed for replies.

3 replies

Shaun.t
Associate III
Oct 31, 2021 2:13 AM UTC

Hi OGaie,

I want to do almost the same thing.

I see no one has replied to your question.

Does it mean that no one has tried this?

Have you been able to test it out. Please share your experience.

Shaun

Tesla DeLorean
Guru
Oct 31, 2021 6:40 AM UTC

It means these type of "can I do x" and "guide me" type questions are frequently ignored because they create a lot of work, and determining these things is part of the project/path you've taken​, so be prepared to do the porting.

The universe of possibilities extends beyond the code one can copy from Google.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Visitor II
Jun 11, 2024 1:04 AM UTC

Hello, 

 

Have you had any luck with this project? I am attempting to perform a similar setup. 

 

Thank you, 

 

Giacomo