Skip to main content
Nikhil Gayke
Associate III
Jan 24, 2022 10:12 AM UTC
Question

how to getting started with STEVAL-IDB011V1 and which tool is used to flash the code and edit the code.

please provide the link and document.@Agnieszka Stawiarska​ @Salvo​ @Salvo​ @Sebastien DENOUAL​ @Salvatore DI SALVO​ @Community member​ 

    This topic has been closed for replies.

    8 replies

    Sebastien DENOUAL
    ST Employee
    Jan 24, 2022 10:19 AM UTC

    HI @Nikhil Gayke​ ,

    I would advise to install at first BlueNRG-LP SDK : https://www.st.com/content/st_com_cx/en/products/embedded-software/evaluation-tool-software/stsw-bnrglp-dk.html

    You can start at first by launching Navigator tools which allow to browse package and code examples in a user friendly way.

    In SDK package, there is also a full documentation with links to different Application notes, Datasheet, schematics, ..... as well as code examples description.

    Hope it helps !

    Regards,

    Sebastien.

    Mario1
    Visitor II
    Apr 29, 2022 12:14 PM UTC

    Hi @Sebastien DENOUAL​ , is it available the Cubemx pack for this board?

    Thanks in advance

    Sebastien DENOUAL
    ST Employee
    Apr 29, 2022 3:23 PM UTC

    Hi @Mario​ ,

    No, CubeMX is dedicated to STM32 family and do not support BleuNRG-LP currently.

    Anyway, there are some alternative for BlueNRG family's that are presented in this thread : CubeMX for BlueNRG LP (st.com)

    Regards,

    Sebastien.

    Mario1
    Visitor II
    Apr 29, 2022 3:40 PM UTC

    @Sebastien DENOUAL​  Many thanks for your quickly answer. I already tested some project with wise studio and have some issue to debug them: Error connecting DP: cannot read IDR... So I decided to start step by step from the skeleton. Any advice?

    Sebastien DENOUAL
    ST Employee
    Apr 29, 2022 3:58 PM UTC

    Hi Mario,

    This might be link to low power and sleep mode management.

    Indeed, if SleepMode is activated on your device, you can not attached CMSIS debug probe.

    To make sure cortex-MO of BleuNRG-LP is activated :

    • Press and hold Push1 button of STEAVL-IDB11
    • Press Reset button
    • Release Push1 button

    At this level, you should be able to flash and debug.

    Of course during development/evaluation phase, you can deactivate sleep mode by cmmenting call to HAL_PWR_MNGR_Request() in main loop.

    Regards,

    Sebastien.

    Mario1
    Visitor II
    May 3, 2022 11:17 AM UTC

    @Sebastien DENOUAL​ Many thanks, your solution work for me. I'd like to take advantage of your kindness to ask you another question...Is the STSW-BNRGLP-Mesh example here available for Wise Studio toolchain? If not, can you give me some guidance on how to convert it for wise?

    Thanks in advance

    Sebastien DENOUAL
    ST Employee
    May 3, 2022 11:43 AM UTC

    Hi @Mario​ ,

    Thanks for feedback.

    About this mesh package, Wise is not supported as of today (I didn't check if this package is fully compliant with arm-gcc).

    Hence, I would advise to use KEIL IDE for which a free license is available :

    > https://www2.keil.com/stmicroelectronics-stm32/mdk

    Regards,

    Sebastien.

    Mario1
    Visitor II
    May 21, 2022 3:51 PM UTC

    @Sebastien DENOUAL​  Many thanks...

    I have another problem: Cannot see any printf in the debug viewer. I'm using Keil and selected CMSIS-DAP as debugger but in the trace setting the option "Trace enable" is gray, so i cannot enable it. by some searching i found that the CMSIS-DAP version has to be at least 1.1 to enable tracing. I have the v1... How to upgrade it?  

    0693W00000NqPJEQA3.jpg0693W00000NqPJJQA3.jpg