Skip to main content
dimitar
Associate
Jan 9, 2015 5:46 PM UTC
Question

How to customize the advertising packet?

Posted on January 09, 2015 at 18:46

Hi,

I'm trying to customize the advertising packet, but it's unsuccessful so far.

I use STEVAL-IDB002V1

BlueNRG HW v3.0

BlueNRG FW v6.4

Motherboard FW v1.4

Since the command ACI_GAP_SET_DISCOVARABLE doesn't give much options I've tried to use  HCI_LE_SET_ADVERTISING_PARAMETERS , HCI_LE_Set_Advertizing_Data, HCI_LE_SET_ADVERTISE_ENABLE.

The response to  HCI_LE_SET_ADVERTISING_PARAMETERS and HCI_LE_SET_ADVERTISE_ENABLE is Unknown HCI Command.

Are these supported commands?

Is there any other way to customize the advertising and scan packet?

Thanks

This topic has been closed for replies.

11 replies

lucaleonardi.919
Visitor II
Jan 22, 2016 10:43 AM UTC
Posted on January 22, 2016 at 11:43

Hi,

I need to use an X-NUCLEO-IDB05A1 on (STEVAL-IDB002V1) RF MOTHERBOARD (vers 3.0). Don't I may connect them with jumper cable male to female?

Using X-NUCLEO-IDB05A1 can I sending broadcast messages without the use of the advertisment? I need to have a device that send broadcast messages and observer the messages of the other device.

Thanks