Skip to main content
hardware
Associate III
Feb 17, 2017 11:48 PM UTC
Solved

How to compute the best connection interval?

Posted on February 18, 2017 at 00:48

Hi,

My BlueNRG-MS, running 7.2c, acts both as a central and a peripheral (mode 4). How should I select the advertizing min and max intervals for the peripheral as well as the connection min and max intervals for the central? There seem to be a relationship between them, but I'm not sure I understand it.

I'm trying to get the minimal connection interval for the central role, while ensuring proper connectivity for the peripheral.

LE_Scan_Interval and LE_Scan_Window seems also to come into play...

Right now, I'm testing different values through trial and error, but if there is a mathematical relationship between those, I'd like to know it.

Thanks!

#bluenrg-ms
    This topic has been closed for replies.
    nick239955_stm1_st
    Associate II
    Feb 26, 2017 10:25 PM UTC
    Posted on February 26, 2017 at 23:25

    I have also been experimenting with different connection / scan interval combinations and found some useful guidelines in the BlueNRG programming manual (

    http://www.st.com/content/ccc/resource/technical/document/programming_manual/1c/7e/d3/a6/d0/52/4a/35/DM00141271.pdf/files/DM00141271.pdf/jcr:content/translations/en.DM00141271.pdf

    For Example, this is from section 4.3:

    4. Every time you start Advertising:

    a) If Direct Advertising, choose Advertising_Interval_Min = Advertising_Interval_Max

    = integer multiple of the shortest allocated connection interval

    b) If not Direct Advertising, choose Advertising_Interval_Min =

    Advertising_Interval_Max such that (Advertising_Interval_Min + 5ms) is an integer

    multiple of the shortest allocated connection interval

    Hope this helps

    2 replies

    Andrea Palmieri
    ST Employee
    Feb 23, 2017 10:43 AM UTC
    Posted on February 23, 2017 at 11:43

    Hi,

    On

    https://github.com/ARMmbed/ble-x-nucleo-idb0xa1

     you can find a wrapper library for BlueNRG-MS.

    In particular, the BlueNRGGap class handles the computation of parameters related to Advertising:

    BlueNRGGap::setAdvParameters()

    and Connection:

    BlueNRGGap::setConnectionParameters

    ()

    Hope that helps.

    nick239955_stm1_st
    Associate II
    Feb 26, 2017 10:25 PM UTC
    Posted on February 26, 2017 at 23:25

    I have also been experimenting with different connection / scan interval combinations and found some useful guidelines in the BlueNRG programming manual (

    http://www.st.com/content/ccc/resource/technical/document/programming_manual/1c/7e/d3/a6/d0/52/4a/35/DM00141271.pdf/files/DM00141271.pdf/jcr:content/translations/en.DM00141271.pdf

    For Example, this is from section 4.3:

    4. Every time you start Advertising:

    a) If Direct Advertising, choose Advertising_Interval_Min = Advertising_Interval_Max

    = integer multiple of the shortest allocated connection interval

    b) If not Direct Advertising, choose Advertising_Interval_Min =

    Advertising_Interval_Max such that (Advertising_Interval_Min + 5ms) is an integer

    multiple of the shortest allocated connection interval

    Hope this helps