Skip to main content
Oktopus15
Associate
Sep 2, 2022 11:06 AM UTC
Solved

How do I select different output voltages from the STUSB4500 without using a microcontroller?

I want to use a STUSB4500LBJR for USB-C power delivery. On the datasheet stands that connecting the I2C lines is optional and in another datasheed of the STUSB4500 stands that I don't have to use a microcontroller. But I cannot find information about choosing a voltage output I want from the STUSB4500 on the internet.

    This topic has been closed for replies.
    Benoit FORETBest answer
    ST Employee
    Sep 2, 2022 12:09 PM UTC

    Hello Oktopus15,

    take care that STUSB4500LBJR is Type-C only for 5V, up to 3A applications.

    STUSB4500BJR is USB-C + PD capable (up to 20V, 5A):

    0693W00000SuNvdQAF.png 

    If you need to change STUSB4500 power profiles, 2 options:

    1°) customize once the Non Volatile Memory (check this software package: STSW-STUSB004)

    2°) or do it on the fly from your application MCU: STSW-STUSB003

    Rgds,

    Benoit

    1 reply

    Benoit FORETBest answer
    ST Employee
    Sep 2, 2022 12:09 PM UTC

    Hello Oktopus15,

    take care that STUSB4500LBJR is Type-C only for 5V, up to 3A applications.

    STUSB4500BJR is USB-C + PD capable (up to 20V, 5A):

    0693W00000SuNvdQAF.png 

    If you need to change STUSB4500 power profiles, 2 options:

    1°) customize once the Non Volatile Memory (check this software package: STSW-STUSB004)

    2°) or do it on the fly from your application MCU: STSW-STUSB003

    Rgds,

    Benoit