Skip to main content
Ahamed Faize
Associate
Dec 20, 2021 9:33 AM UTC
Solved

Hi team, We have used TESEO-LIV3F Receiver in our design. We are planning to use Active Antenna with this module. Active Antenna Part No. is ECHO27/0.1M/IPEX/S/S/15. Please suggest us how to interface the active Antenna with this module. Regards Faiz

..

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Dec 22, 2021 7:59 AM UTC

    You can look at the X-NUCLEO-GNSS1A1 as an example, where, in addition to the inductor L2 (56nH) and the block capacitor C9 (56pF), a bidirectional single line ESD TVS protection diode is used. You can find all information under the tab CAD Resources: schematics, bom, etc.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    3 replies

    Peter BENSCH
    ST Technical Moderator
    Dec 20, 2021 12:32 PM UTC

    Please have a look at UM2832, section 8.2. where the coupling of an active antenna is shown. It is a different TESEO module, but the principle is identical. The DC supply of the antenna is fed in via an LC element, decoupled from the received signal. In addition, the UM2832 shows how Ant_OFF can optionally be used to switch this DC.

    Good luck!

    If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Ahamed Faize
    Associate
    Dec 21, 2021 6:14 AM UTC

    Thanks, Peter!

    Please suggest us how to select the values for the DC coupling components (inductor & bypass capacitor & AC coupling component(capacitor in the RF line).

    Regards,

    Faize

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Dec 22, 2021 7:59 AM UTC

    You can look at the X-NUCLEO-GNSS1A1 as an example, where, in addition to the inductor L2 (56nH) and the block capacitor C9 (56pF), a bidirectional single line ESD TVS protection diode is used. You can find all information under the tab CAD Resources: schematics, bom, etc.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.