Skip to main content
merivel
Associate
Jun 5, 2023 2:35 PM UTC
Question

Hi, in sw package BlueNRG-2 “over-the-air�? (OTA) firmware upgrade what happened in case : 1 - power failure during upgrade? 2 - lost of BLE during update? in configuration OTA service manager framework

..

This topic has been closed for replies.

3 replies

merivel
merivelAuthor
Associate
Jun 5, 2023 3:59 PM UTC

.

Winfred LU
ST Employee
Jun 6, 2023 5:59 AM UTC

Refer to:

AN4869: The BlueNRG-1, BlueNRG-2 BLE OTA (over-the-air) firmware upgrade

With the OTA service manager framework, the firmware will be corrupted. The user has to restart the OTA upgrade procedure.

With the reset manager and the higher/lower application approach, the new firmware is corrupted too. But, the old firmware application can still work, since only (approximately) half of the flash memory was to be upgraded.

merivel
merivelAuthor
Associate
Jun 6, 2023 8:37 AM UTC

When BLE communication is lost, reestablishing the OTA upgrade procedure happens automatically after a timeout or requires a manual reset?