Skip to main content
Visitor II
Nov 13, 2024 3:11 PM UTC
Question

Help needed for STEVAL-BFA001V2B connection to IO-Link master

Hi,

I am trying to connect the STEVAL-BFA001V2B to a siemens ET-200SP IO-Link master. I have flashed the MCU with the STEVAL-BFA001V2_PredMaint_IOL_V1.1.0 using the STM32Cube Programmer. The PLC's IO link configurator connects with the BFA001V2B however is shows an error (0x 1800 - Event ALARM on axis X in SUB1) and (0x 180A - Event ALARM on axis Z in SUB2). I have attached images showing the errors and of the process data being all 0.

I would really appreciate any help in solving this issue.

 

Thank you.

image (1).png

image (2).png

This topic has been closed for replies.