Skip to main content
AThom.17
Associate
Jun 17, 2019 7:01 AM UTC
Question

HCF4010Y CAN USE AS CMOS TO TTLCONVERTER

Hello,

Iam using HCF4010 for my project. Can i use this as CMOS to TTL converter?

Also for high speed switching or for high speed signal is there any issue for using the same ic(Please find the attached image,4 GPIO & 2 spi lines were used)

0690X000008ilGUQAY.jpg

    This topic has been closed for replies.

    2 replies

    Ozone
    Principal
    Jun 17, 2019 7:19 AM UTC

    I think not.

    You would have to keep Vcc at 5V, which would not constitute a level shifter.

    If you raise Vcc, the L/H thresholds go up proportionally.

    jrgert
    Associate III
    Sep 16, 2019 2:21 PM UTC

    Datasheet DocID8190 Rev 8 says...

    "It is a non-inverting hex buffer/converter and can be used as a CMOS to TTL logic level converter, "