Skip to main content
KOO
Visitor II
Jul 8, 2021 12:51 PM UTC
Question

Getting STEVAL-BCN002V1B Mems Microphone Streamming Data using Ble protocol on Win10 PC python.

I'm working on a code for streaming STEVAL-BCN002V1B-BlueTile on Windows 10 PC Python.

​

The microphone data is notify property, and when I saw the BLE_SensorDemo.c file through StmIDE, the signal transmission of the microphone was configured as a state machine.

​

If I run my Python code alone on the PC, the microphone signal does not send to the PC. But

​

If you force the app to shut down while receiving microphone signals from the ST_BLE_Sensor app and execute Python code on your PC, you will be able to receive microphone signals.

​

So I want to modify the C file of BLE_SensorDemo so that the STEVAL-BCN002V1B chip itself can send a microphone signal as soon as Bluetooth is connected.

I want to put STEVAL-BCN002V1B into Bluetooth microphone streaming mode when it is powered on.

​

So I revised the C file several times, but it didn't work out, so I asked you a question. Give me some advice on what to do.

Here is Python test Code

------------------------------------------------------------------------------------------------------------

import asyncio

import bleak # bleak

from bleak import BleakClient

address = "D9:D4:30:7E:59:89" #you should change

# service uuid: 00000000-0001-11e1-9ab4-0002a5d5c51b

notity_charcteristic_uuid = "08000000-0001-11e1-ac36-0002a5d5c51b"

def notify_callback(sender: int, data: bytearray):

print('sender: ', sender, 'data: ', data)

async def run(address):

async with BleakClient(address, timeout=5.0) as client:

print('connected')

services = await client.get_services()

for service in services:

for characteristic in service.characteristics:

print(' uuid:', characteristic.uuid)

print(' handle:', characteristic.handle)

print(' properties: ', characteristic.properties)

if characteristic.uuid == "08000000-0001-11e1-ac36-0002a5d5c51b":

print('try to activate notify.')

while(1):

await client.start_notify(characteristic, notify_callback)

if client.is_connected:

print('try try try')

await asyncio.sleep(1)

print('try to deactivate notify.')

await client.stop_notify(notity_charcteristic_uuid)

print('disconnect')

loop = asyncio.get_event_loop()

loop.run_until_complete(run(address))

print('done')

----------------------------------------------------------------------------------------------------------

This topic has been closed for replies.