Skip to main content
OLAAO.1
Visitor II
Jul 13, 2020 9:52 AM UTC
Question

Getting started with X-Nucleo-IDW01M1, wifi connectevity + Nucleo-F446ZE

Hello,

I want to add the wifi module to my Nucleo-F446ZE board, and for that I'm using X-Nucleo-IDW01M1.

I know that the connection between the Nucleo BOARD and the WIFI module goes through UART. So, we must configure UART1 for the connection between the Nucleo board and the wifi module and then uart 2 for the connection with the PC. I looked for examples of TUTO, documentation, project carried out on other nucleo cards to get an idea on the configuration on STM32Cube and the AT commands used but I can't find anything. Is it possible to create a project and develop the wif module on STM32CUBEIDE with idw01M1? Should I use another module like ESP8266? Would someone have a track for this type of configuration, an example with another Nucleo board or anything that could help me with this problem?

Thinks :)

This topic has been closed for replies.

1 reply

Piranha
Principal III
Jul 15, 2020 9:24 AM UTC

UM1695