Skip to main content
kukushonok
Associate III
August 11, 2014
Question

Flash recovery

Posted on August 11, 2014 at 11:24

Hi,

I'm developing a device based on the BlueNRG. 

I worked on the support of flash BlueNRG from my firmware,  but during a flash error occurred (probably due to an incorrect program address). After flash failed BlueNRG does not respond, as in my firmware and through the RF MOTHERBOARD vers. 3.0 (BLUENRG_GUI.exe).

Is there a way to restore the firmware? 

Maybe can I download the firmware via JTAG?

Software engineer, Andrei Kukenov.

Regards. 

#recovery #flash #bluenrg #image
This topic has been closed for replies.

14 replies

gabor2
Visitor II
August 12, 2014
Posted on August 12, 2014 at 10:46

Hi Andrei,

I'm not part of the ST team, I'm a developper. But I think I can answer to your problem. If you check the attached pdf you can see that the 8., 9., and the pins are the JTAG pinouts. If you connect them to a programmer you might be able to program the original firmware which can be donwloaded from the ST's website. The firmwares are located in the BlueNRG GUI's installation folder.

Best regards,

G

________________

Attachments :

DM00097377.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Ht2r&d=%2Fa%2F0X0000000aJF%2FXa0kMuJiCfxBG.I5_kQ8Qf.szs2ktVaPqPdmJbZ6cUs&asPdf=false
kukushonok
Associate III
August 12, 2014
Posted on August 12, 2014 at 16:11

Thank you very much for your reply. I have already connected to the module via the j-link, but I don't know how to flash the firmware, so much so programmer does not know the device with this id, and therefore can not erase and flash. Also it is not clear to what address I need to flash up the firmware...

Regards

gabor2
Visitor II
August 13, 2014
Posted on August 13, 2014 at 10:32

Hi,

You're right. That won't be easy since there is no data available in any document which describes the structure of flash (or I cannot find it). So sorry that I can't help you.

g

marchese.graziella
Visitor II
November 20, 2014
Posted on November 20, 2014 at 15:40

Hi All,

To update the firmware inside the BlueNRG, you have to use the BLUENRG_GUI. To use the GUI, the VCOM firmware (BlueNRG_VCOM_1_3.hex) must be flashed inside the STM32L.

To understand how to proceed, please read the document ''User manual BlueNRG development kits'' (UM1686) that you can download at the following link:

 

http://www.st.com/st-web-ui/static/active/jp/resource/technical/document/user_manual/DM00099259.pdf

.

Regards,

Graziella Marchese

Scott Löhr
Senior III
January 7, 2015
Posted on January 07, 2015 at 23:45

Dear Marchese / ST:

I have X-NUCLEO-IDB04A1. Accessing f/w version by running Virtual COM port sample app and BlueNRG GUI v1.6.0 showed this:

HW v3.0

FW v6.3

So I updated FW to v6.4 and now the advertising / BLE is broken. I tried both of these:

bluenrg_6_4_Mode_2-16MHz-XO32K.img

bluenrg_6_4_Mode_2-32MHz-XO32K.img

Neither one works. The BlueNRG is apparently still responsive across the SPI bus, as now the BlueNRG GUI v1.6.0 shows this:

HW v3.0

FW v6.4

I suspect that I need a N.img image for this newer board, as the images referenced above are from a BlueNRG DK 1.6.0 installation, whereas the sample apps used to talk to it are from a X-CUBE-BLE1 installation.

Thanks for any help...

ronan
Visitor II
January 9, 2015
Posted on January 09, 2015 at 13:40

Note: I am not with ST, but I know that some of the HCI response structures  have 

changed between 6.3 and 6.4 so your application needs to be updated. 

The 

EVT_BLUE_GAP_DEVICE_FOUND structure has changed -it now reports RSSI and scan data (I think). If you download the latest SDK it has version 1.6.0  code, you are probably using SDK 1.5.0

marchese.graziella
Visitor II
January 21, 2015
Posted on January 21, 2015 at 16:56

Hi,

which nucleo motherboard are you using? L1, L0, F4?

which VCOM firmware have you loaded on the motherboard?

Assuming that the fw image ''bluenrg_6_4_Mode_2-16MHz-XO32K.im''g has been correctly loaded (as showed in the GUI), have you tried to run basic command as GATT_INIT, GAP_INIT with the GUI?

Are they run with success? (Check the HCI_COMMAND_COMPLETE Status =Success)?

If yes, the BlueNRG fw upgrade should be ok, so another test that you could to do is to set the TX power as follow:

ACI_HAL_SET_TX_POWER_LEVEL(0x01,0x04) and verify if the device is correctly advertising or not.

The Tx Power settings address an issue which is documented in the device errata (see section 1.3). You can download the document at the following link:

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/errata_sheet/DM00133230.pdf

Best Regards,

Graziella Marchese

Scott Löhr
Senior III
January 21, 2015
Posted on January 22, 2015 at 00:46

Hello - I have a X-NUCLEO-IDB04A1 mounted onto a Nucleo-STM32F401 and am using the sample apps from the X-CUBE-BLE1 v2.2.

Before programming the X-NUCLEO-IDB04A1 with v6.4, the sample apps would advertise, now they do not. The SPI protocol is still working, just that the BlueNRG no longer is seen over the air. I suspicion that I have programmed a bluenrg v6.4 built for older h/w, a previous sdk. I found the images buried in some ''BlueNRG DK v1.6.0'' which I cannot now find on the ST website - I don't even know where I first ever got it now (I got it legally, either from the ST website or from the installer disc for the ST seminar). Even the GUI messages for ''upgrading the motherboard'' are outdated, talking about verifying that it is in loader mode by an orange LED, the Nucleo-STM32F401 only seems to have a Green LED (and of course the red led indicating power).

Scott Löhr
Senior III
January 21, 2015
marchese.graziella
Visitor II
January 22, 2015
Posted on January 22, 2015 at 09:32

Hi,

the bluenrg fw images is the same for STEVAL-IDB002V1'' and ''X-NUCLEO-IDB04A1'', different is the VCOM firmware loaded on the motherboard. For X-NUCLEO-IDB04A1 you have to load the VCOM firmware related to your STM32F present in the X-CUBE-BLE1package. In anycase, you should try to reload the BlueNRG fw image version 6.3and try if it works.

Regards,

Graziella

Ok, I just found where is this mysterious v1.6.0:

http://www.st.com/web/en/catalog/tools/PF259737

Thanks to this post:

https://my.st.com/public/STe2ecommunities/interface/Lists/Low%20Power%20RF%20Solutions/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2finterface%2fLists%2fLow%20Power%20RF%20Solutions%2fdriver%20and%20application%20built%20for%20BlueNRG&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580008F23D8A934F45B4FB64D6201532EFD99&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Finterface%2FLists%2FLow%2520Power%2520RF%2520Solutions%2FAllItems.aspx&currentviews=10

But that v1.6.0 is for ''STEVAL-IDB002V1'' and I have the new ''X-NUCLEO-IDB04A1'', so the bluenrg images cannot be compatible, yes? And yet they are compatible enough to still drive the SPI interface (but not get over the air advertising)?