Skip to main content
puneetha shankar
Visitor II
Jul 18, 2017 11:59 AM UTC
Question

Firmware Difference in BLUENRG V7.2.c & V7.1.e

Posted on July 18, 2017 at 13:59

i'm working on a

BLUENRG_CSP device and i've retained the ble section similar to the Sensor Tile STLCS01V1,

my BLE is initializing but not advertising.

i'm able to read the device ID,

only difference i can see with respect to Sensor tile is  BLE Firmware version

Sensor Tile Version is 7.2.c

my device version is 7.1.e

can somebody please guide me through, what could be the problem,

also

Can you confirm that 7.1.e is for 32MHZ or 16 MHZ. Should i worry about frequency if so, Is there any option to update the BLE firmware.

Thanks & Regards,

Puneethashankar

    This topic has been closed for replies.