Skip to main content
egoltzman
Senior
May 23, 2016 9:15 AM UTC
Question

Fail to update firmware on BlueNRG-MS X-NUCLEO-IDB05A1

Posted on May 23, 2016 at 11:15

I'm working with the X-NUCLEO-IDB05A1 with the BlueNRG-MS on it.

I follow the quick start guide (Version 1.4) and on the ''Evaluate BlueNRG using a GUI'' section when starting the BlueNRG GUI (Version 1.9) it asked me to upgrade the BlueNRG firmware.

I run the BlueNRG Updater and tried to program the firmware version that come with the BlueNRG DK 1.9.0 under firmware directory (I tried both the 16MHz and the 32MHz) but after a successful (allegedly) flashing at the verify stage it fail in the middle (I tried more then once) with an error message HCITimeoutError.

Please advise

 

#bluenrg-ms
This topic has been closed for replies.