Skip to main content
DLoza.2
Associate III
Feb 25, 2022 9:51 AM UTC
Question

Extended Advertising and Coded PHY in Broadcast Role

Hello,

I'm trying to program a STEVAL-IDB011V1 board with the Broadcast Role, Extended Advertising and Coded PHY. When I run my program, I got this error:

Error in aci_gap_set_advertising_configuration() 0x82

I know that this error is: Invalid parameters passsed at Host layer. But I don't know what I'm doing wrong.

These are my configurations:

// Init the GAP:

aci_gap_init(GAP_BROADCASTER_ROLE, 0x00, 0x08, PUBLIC_ADDR, &service_handle, &dev_name_char_handle, &appearance_char_handle);

// Gap adv configuration

status = aci_gap_set_advertising_configuration

(

0,

GAP_MODE_BROADCAST,

0,

333*0.635,

333*0.635,

ADV_CH_ALL,

PUBLIC_ADDR,

NULL,

ADV_NO_WHITE_LIST_USE,

127,

LE_CODED_PHY,

0,

LE_CODED_PHY,

0,

0

);

Thanks,

Daniel

    This topic has been closed for replies.

    3 replies

    Sebastien DENOUAL
    ST Employee
    Feb 25, 2022 11:20 AM UTC

    Hi @DLoza.2​ ,

    There is a code example for advertising extension usage in BlueNRG-LP SDK.

    > Beacon project - Select "ExtendedAdv" configuration.

    Also, to activate Extended extension, you may have to take care about BLE Stack configuration.

    Indeed, to save RAM/FLAH you can select your BLE stack config and associated BLE features.

    FYI, here are possible BLE stack config :

    • BLE_STACK_FULL_CONF => Possible
    • BLE_STACK_BASIC_CONF => not possible
    • BLE_STACK_SLAVE_DLE_CONF => not possible
    • BLE_STACK_SLAVE_DLE_LE_2M_CODED_CONF => not possible
    • BLE_STACK_CUSTOM_CONF (need to enable CONTROLLER_EXT_ADV_SCAN_ENABLED flag) - custom definition in custom_ble_stack_conf.h

    Regards,

    Sebastien.

    DLoza.2
    DLoza.2Author
    Associate III
    Mar 15, 2022 11:14 AM UTC

    Hello again Sebastien,

    Thanks for your answer. I was already editing the program that you have recommend me. Also I have defined EXT_ADV_PHY, LE_CODED_PHY and BLE_STACK_FULL_CONF, so I don't think the problem is in the stack configuration.

    I have changed some GAP config parameters of the code, but I still have the same error:

    Error in aci_gap_set_advertising_configuration() 0x82

    My new GAP config:

    // Gap adv configuration

    status = aci_gap_set_advertising_configuration

    (

    1,

    GAP_MODE_BROADCAST,

    0,

    (333*1000/625),

    (333*1000/625),

    ADV_CH_ALL,

    PUBLIC_ADDR,

    NULL,

    ADV_NO_WHITE_LIST_USE,

    127,

    LE_CODED_PHY,

    0,

    LE_CODED_PHY,

    1,

    0

    );

    I know that this error is: Invalid parameters passsed at Host layer. But I don't know what I'm doing wrong.

    Regards,

    Daniel

    ajeet
    Associate
    Mar 22, 2022 3:43 PM UTC

    Hi @Sebastien DENOUAL​ can I use same extended advertisement example code for STM32WB55?