Skip to main content
Associate
Jul 10, 2026 7:42 PM UTC
Solved

EVAL-SCS006V1 No Load power consumption

EVAL-SCS006V1 (TSUSB4532) is plugged into a 65W power supply with an in-line USB-C meter. 

With no load attached, the meter reads 20.06V, 0.016A, and 0.321W. What on the board that consumes this much power?

In contrast, an EVAL-SCS006V1 (STUSB4500) is plugged into the same configuration, the meeter reads 20.07V, 0.000A, 0.000W.

Please help me figure this out!

 

t.pBest answer
Associate
Jul 16, 2026 3:43 PM UTC

Hi Didier, 

Sorry for the typo. The STUSB4500 Eval we purchased is EVAL-SCS001V1.

And thank you for pointing out the LEDs. I remeasured everything, it turned out the issue is somewhere with the cables I used, that are not consistent between two brands, and the orientation of the cable when plugged in the USB-C socket.

Thank you again, and please consider the issue resolved.

 

2 replies

Didier HERROUIN
ST Technical Moderator
Jul 16, 2026 3:02 PM UTC

Dear t.p,

The current you observe on EVAL-SCS006V1 is due to the LEDS consumption (20V through the LEDs with 22kohms in series). Of course, these LEDs will not be present in your final design.
On the STUSB4500 board (the reference you provided is not the correct one), I suppose that no LED is switched on.

Best regards,

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
t.pAuthorBest answer
Associate
Jul 16, 2026 3:43 PM UTC

Hi Didier, 

Sorry for the typo. The STUSB4500 Eval we purchased is EVAL-SCS001V1.

And thank you for pointing out the LEDs. I remeasured everything, it turned out the issue is somewhere with the cables I used, that are not consistent between two brands, and the orientation of the cable when plugged in the USB-C socket.

Thank you again, and please consider the issue resolved.