Skip to main content
Ayden
Associate II
Jan 28, 2022 5:06 AM UTC
Question

Error occurs in WISE-Studio when migration to BlueNRG-345xy.

An error occurs in WISE-Studio when migration occurs from BlueNRG-355xy to BlueNRG-345xy.

I worked with reference to "How to move a demo application from BlueNRG-355xy to BlueNRG-345xy" in the https://www.st.com/resource/en/user_manual/dm00711446-bluenrglp-development-kits-stmicroelectronics.pdf document.

-------------------------------------------------------------------------------------------------------------------

• WiSE-Studio toolchain: – open the WiSE-Studio .cproject file and replace BlueNRG-355 with BlueNRG-345 – in [Projects][Properties][C/C++ Build][Settings][Tool Settings][GCC C Compiler][Preprocessor] [Defined Symbols], add CONFIG_DEVICE_BLUENRG_345 – in [Projects][Properties][C/C++ Build][Settings][Tool Settings][GCC Linker][Miscellaneous][Other linker flags], add CONFIG_DEVICE_BLUENRG_345=1 

-------------------------------------------------------------------------------------------------------------------

make -j4 all 

Building target: BLE_MultipleConnections.elf

Invoking: GCC Linker

arm-none-eabi-gcc -mcpu=cortex-m0plus -mthumb -mfloat-abi=soft -nostartfiles -nodefaultlibs -Wl,--gc-sections -Wl,-Map="BLE_MultipleConnections.map" -T"../BlueNRG_LP.ld" -L../../../../../../Middlewares/ST/Bluetooth_LE/Library -L../../../../../../Middlewares/ST/cryptolib -Wl,--cref, CONFIG_DEVICE_BLUENRG_345=1 --specs=nano.specs -o "BLE_MultipleConnections.elf" -Wl,--start-group @"objects.list" -lbluenrg_lp_stack -lcrypto -lm -lc -Wl,--end-group

arm-none-eabi-gcc: error: CONFIG_DEVICE_BLUENRG_345=1: No such file or directory

make: *** [BLE_MultipleConnections.elf] Error 1

makefile:57: recipe for target 'BLE_MultipleConnections.elf' failed

"make -j4 all" terminated with exit code 2. Build might be incomplete.

14:11:12 Build Failed. 2 errors, 0 warnings. (took 1s.169ms)

-------------------------------------------------------------------------------------------------------------------

Which part should be modified?

    This topic has been closed for replies.

    3 replies

    Sebastien DENOUAL
    ST Employee
    Feb 3, 2022 2:39 PM UTC

    Hi @Ayden​ ,

    Unfortunately, issue you noticed is vali and will be soon fixed within next SDK release.

    Same subject was discussed here : https://community.st.com/s/feed/0D53W00001Kyo3ESAR

    As I wrote in other thread, possible workaround are :

    Thanks for your understanding.

    Regards,

    Sebastien

    Sebastien DENOUAL
    ST Employee
    Feb 3, 2022 3:05 PM UTC

    Hi again @Ayden​ ,

    Let me share with you proper change to switch a project to BlueNRG-345 with Wise :

    • open the WiSE-Studio .cproject file and replace BlueNRG-355 with BlueNRG-345
    • in [Projects][Properties][C/C++ Build][Settings][Tool Settings][GCC C Compiler][Preprocessor] [Defined Symbols], add CONFIG_DEVICE_BLUENRG_345
    • in [Projects][Properties][C/C++ Build][Settings][Tool Settings][GCC Linker][Miscellaneous][Other linker flags], add -Wl,--defsym=CONFIG_DEVICE_BLUENRG_345=1

    0693W00000JOR6oQAH.png 

    Regards,

    Sebastien.

    Ayden
    AydenAuthor
    Associate II
    Feb 6, 2022 11:16 PM UTC

    Hi Sebastien

    Your comment helped me a lot. Thank you.