Skip to main content
ASay.1
Associate II
Nov 21, 2023 11:33 AM UTC
Question

Enabling OOK in S2LP

Hello I have a confusion when the OOK is enabled in the S2LP chip.

In datasheet section 5.4.2 writes:

The ASK selection depends on power ramping enable.

When OOK is selected, a bit '1' is transmitted with a programmed power, set by register PA_POWER[PA_LEVEL_MAX_INDEX], and a bit '0' is transmitted without output power (PA off) and specified
by the register PA_POWER[0]. In case PA_POWER[0] = 0 then

In case PA_POWER[0] = 0 then the modulation will be OOK, otherwise when PA_POWER[0] is not set to zero the modulation will be ASK.

In datasheet  section 5.6.1 writes:

For OOK modulation, the signal is abruptly switched between two levels only: no power and maximum. This mode is obtained setting the PA_RAMP_EN=0.

Statement "In case PA_POWER[0] = 0 then the modulation will be OOK, otherwise when PA_POWER[0] is not set to zero the modulation will be ASK." looks not clear to me. Does it mean even though PA_RAMP_EN is 0, setting PA_POWER[0] to a non-zero value makes it ASK?

 

This topic has been closed for replies.