Skip to main content
RMoc.1
Associate II
Mar 16, 2023 1:24 PM UTC
Question

Enable Data Length Extension (DLE) and increase MTU size BlueNRG M2

I am using BLUENRG M2SA and would like to enable data length extension and increase the MTU size. I read the PM0257 programming manual and made the following changes.

#define CLIENT_MAX_MTU_SIZE 185
 
void hci_le_connection_complete_event(uint8_t Status,
 uint16_t Connection_Handle,
 uint8_t Role,
 uint8_t Peer_Address_Type,
 uint8_t Peer_Address[6],
 uint16_t Conn_Interval,
 uint16_t Conn_Latency,
 uint16_t Supervision_Timeout,
 uint8_t Master_Clock_Accuracy)
{
 connected = true;
}
 
void aci_att_exchange_mtu_resp_event(uint16_t Connection_Handle,
 uint16_t Server_RX_MTU)
{
 if (Server_RX_MTU <= CLIENT_MAX_MTU_SIZE)
 {
 write_len = Server_RX_MTU - 3;
 }
 else
 {
 write_len = CLIENT_MAX_MTU_SIZE - 3;
 }
 
 if ((mtu_exchanged_wait == 0) || ((mtu_exchanged_wait == 1)))
 {
 if (mtu_exchanged_wait == 0)
 {
 mtu_exchanged_wait = 2;
 }
 mtu_exchanged = true;
 }
}
 
void hci_le_data_length_change_event(uint16_t Connection_Handle,
 uint16_t MaxTxOctets,
 uint16_t MaxTxTime,
 uint16_t MaxRxOctets,
 uint16_t MaxRxTime)
{
}
 
 
static void User_Process(void)
{
 tBleStatus ret;
 
 if (connected)
 {
 if ((mtu_exchanged == false) && (mtu_exchanged_wait == 0))
 {
 mtu_exchanged_wait = 1;
 ret = aci_gatt_exchange_config(connection_handle);
 if (ret != BLE_STATUS_SUCCESS)
 {
 // Handle error
 }
 
 ret = hci_le_set_data_length(connection_handle, CLIENT_MAX_MTU_SIZE, TX_OCTETS_TO_TIME(CLIENT_MAX_MTU_SIZE));
 if (ret != BLE_STATUS_SUCCESS)
 {
 // Handle error
 }
 }
 }
}
 
void send_data(void)
{
 aci_gatt_update_char_value_ext(handle,
 serv_handle,
 char_handle,
 1, 170, 0, 170, buff);
}

I am trying to send 170 bytes of data per packet. Is the above method correct?

I am not getting hci_le_data_length_change_event callback when connected to some phones. The phone specs mention that it has BLE v4.2, still unable to get callback. How to resolve this issue?

This topic has been closed for replies.

4 replies

Billy OWEN
ST Employee
Mar 17, 2023 4:48 PM UTC

Hi @RMoc.1​ 

The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.

Regards,

Billy

RMoc.1
RMoc.1Author
Associate II
Mar 20, 2023 10:19 AM UTC

Thanks for the update @Billy OWEN​.

Just to add, I have flashed the module with DTM_SPI_M2SA firmware from BLUENRG1-DK -- BlueNRG-1, BlueNRG-2 DK SW package v3.2.3 to use as a network co processor. Also the HS_SPEED_XTAL = HS_CRYSTAL_32MHZ, LS_SOURCE = LS_SOURCE_32KHZ & SMPS_INDUCTOR = SMSP_10uH changes are made in the firmware.

Visitor II
Nov 21, 2024 4:45 PM UTC

Dear ST, I have the same issue. I applied all the changes suggested in the application note pm0257 and also used by user RMoc.1 above. However, even if I can transmit data > 20 bytes, I am not able to receive data > 20 bytes. Can you please help?

Thank you.