Skip to main content
satyam9896
Associate III
Mar 7, 2025 3:20 PM UTC
Question

DTM test for RF testing (Enable DTM Mode for BLE-SPBTLE-RF0 via SPI1 on STM32L053)

Hi Everyone,
I am working on enabling Direct Test Mode (DTM) for BLE-SPBTLE-RF, which is connected to my STM32L053 via SPI1 on a custom PCB. The goal is to perform RF testing so I can submit the board for regulatory certification.

Hardware Setup:

  • MCU: STM32L053
  • BLE Module: SPBTLE-RF
  • Connection Interface: SPI1
  • Available Debug Pins: SWDIO & SWCLK (Used for ST-LINK flashing & debugging)
  • Custom PCB: Already assembled, so I cannot access additional UART/SPI pins easily or can design(only things i can do is i take out connection from  the ble pads by soldering jumpers if req)

    Challenges:

    1. Since SPI1 is used for communication with the BLE module, can I still enable DTM mode without a direct UART connection?
    2. The official DTM firmware expects an HCI UART interface. Is there an alternative way to send DTM commands via SPI?
    3. Given my limited access to only SWDIO & SWCLK, is there a way to configure the BLE module into DTM mode through firmware modifications on STM32L053?

      What I Need:

      • Steps to enable DTM mode on SPBTLE-RF via SPI or any other methot if possible by soldering the wires jumpers.
      • Any firmware or workaround to control DTM commands over SPI instead of UART.
      • Alternative debugging or testing approaches considering my hardware limitations.
      • How to interface the board with BlueNRG GUI or BEAM (BlueNRG Analyzer Mobile app) for RF testing from bypassing the stm32 to ble or if possible through stm32 to ble.
This topic has been closed for replies.

1 reply

satyam9896
Associate III
Mar 13, 2025 6:07 AM UTC

Hi, If any one help me out please help me.