Skip to main content
nicolai86
Associate II
Apr 28, 2020 5:11 PM UTC
Question

Does the STUSB4500 require additional ESD protection?

Per the STUSB4500 datasheet it provides basic ESD protection:

ESD: 3 kV HBM - 1.5 kV CDM

I was wondering if it's still useful to combine the STUSB4500 with a TCPP01-M12

System-level ESD protection for USB type-C connector pins (CC1, CC2), compliant with IEC 61000-4-2 level 4 (±8 kV contact discharge, ±15 kV air discharge)

I can't find any data for this in either datasheet. Does this make sense in practice, having both ICs on your board?

    This topic has been closed for replies.