Skip to main content
rds-tmeyer
Associate II
Jun 15, 2021 3:49 PM UTC
Question

Does flash readout protection activation via bootloader protect SWD read as well on BlueNRG-232?

I have a BlueNRG2 firmware that includes critical application level encryption keys. It is flashed using the bootloader. If I activate the flash readout protection using the bootloader commands (0x82), is the flash protected from readout through SWD as well?

This topic has been closed for replies.