Skip to main content
paolo23
Associate II
Aug 31, 2015 5:13 PM UTC
Question

Delay between SPWF01 messages

Posted on August 31, 2015 at 19:13

Hi everybody, I'm evaluating the SPWF01SA and I'm wondering if there is a minimum delay between messages useful to determine the end of a transmission, ex. between the response to a command and a following WIND?

Thanks

Paolo
    This topic has been closed for replies.

    4 replies

    Gerardo GALLUCCI
    ST Employee
    Sep 1, 2015 11:22 AM UTC
    Posted on September 01, 2015 at 13:22

    Ciao Paolo,

    AT-commands and WINDS are not related. I mean: SPWF have synch indications (OK/ERROR) and asynch indications (+WIND).

    - When you run an AT-command, you have to expect OK or ERROR reply, than go on to next AT-command;

    - WINDs management must be in a ''background task'', since thay can happen in every moment.

    Note: WINDs are never delivered between an AT-command and related OK/ERROR reply.

    jerry

    paolo23
    paolo23Author
    Associate II
    Sep 1, 2015 1:07 PM UTC
    Posted on September 01, 2015 at 15:07

    Thank you, Jerry.

    As the command guide says, asynchronous messages can be sent at any time but not between commands and responses.

    This means that a pending asynchronous message can theoretically be queued to a response and become a single transfer with it. In this case, a time-out in reception would not be enough to separate the messages. Is that right?

    Paolo

    Gerardo GALLUCCI
    ST Employee
    Sep 1, 2015 1:24 PM UTC
    Posted on September 01, 2015 at 15:24

    Pending WINDs are queued, and printed after OK/ERROR.

    Module side, they are always multiple transfers (2 or more printfs).

    Using STM32 as external host: I suggest an UART management by DMA through a circular buffer, and an interrupt on UART IDLE detection. You can check circular buffer (and parse it!) when curcular buffer is [half]full, or when idle interrupt occurrs on UART.

    If you prefer a different approach, estimate your timeout on used baudrate. Remember that every WIND from SPWF starts and ends with a CrLf.

    Hope to be useful.

    ciao

    jerry

    paolo23
    paolo23Author
    Associate II
    Sep 2, 2015 6:24 AM UTC
    Posted on September 02, 2015 at 08:24

    Yes, you are.

    Ciao,

    Paolo