Skip to main content
FChou
Associate II
Jan 28, 2019 12:29 PM UTC
Question

Data rate value and TX information from BlueNRG1 Mesh?

hi,

i am searching for the information about the data rate and TX power value in Mesh code where can i find this information ?

In datasheet the air data rate is about 1 Mbit/s is this data rate the same like for the BlueNRG-1 Mesh ?

Thank you

This topic has been closed for replies.

1 reply

alok
Visitor II
Feb 5, 2019 1:37 PM UTC

Did you review the function  Appli_BleSetTxPowerCb for setting the Tx Power ?

The BLE-Mesh is for low data rate applications. You can consider 8bytes application data being transferred per 20ms of advertisement interval. Then the size of Mesh will define the total application throughput