Skip to main content
Nandy K
Associate III
Oct 19, 2015 2:54 PM UTC
Question

Data Mode SPWF01SC.11

Posted on October 19, 2015 at 16:54

Hai Guys !

I am using SPWF01SC.11 , I have connected this with the micro controller via UART.

From the micro controller I am sending a command AT+S.SOCKD= port number through UART.

Now my WiFi module received the command and entered into the data mode.

I know the IP address and port number of the wifi module now and  i connected it from my computer.

Now I have a sent the  string ' Hai' from my computer and I can see the string in the data mode on hyper terminal.

My question :  

1. what will happen on the wifi module once it received the string in the data mode ?

2. will it send the string through UART ?

#spwf01s-wifi #spwf01sa-wifi-scan-command
    This topic has been closed for replies.

    2 replies

    Nickname3786_O
    Visitor II
    Oct 19, 2015 4:46 PM UTC
    Posted on October 19, 2015 at 18:46

    Hi,

    when your socket client connects to the module, two indications will be printed on the UART:

    +WIND:61:Incoming Socket

    Client:[client IP]

    +WIND:60:Now in Data Mode

    After that, all the data sent from the client will be directly printed on the UART of the module.

    Please refer to the LAB13 of the Hands-on for details (http://www.st.com/web/en/catalog/tools/PF261605)
    Nandy K
    Nandy KAuthor
    Associate III
    Oct 19, 2015 5:03 PM UTC
    Posted on October 19, 2015 at 19:03

    Thanks a lot salva !!!!!!