Skip to main content
IJenk.1
Associate II
Apr 28, 2022 4:20 PM UTC
Question

CubeMX for BlueNRG LP

Can you use CubeMX to generate init code for the LP SoC?

I am integrating an LP SoC into a custom PCB and not sure what all I need to init?

    This topic has been closed for replies.

    3 replies

    Sebastien DENOUAL
    ST Employee
    Apr 29, 2022 6:54 AM UTC

    HI @IJenk.1​ ,

    CubeMX is dedicated to STM32 familly and does not support BlueNRG-LP.

    Anyway, some free IDEs are available : KEIL (free license) or WiseStudio (Eclipse based - armgcc)

    To start your development, I would advise to install BlueNRg-LP SDK : STSW-BNRGLP-DK

    It includes multiple code examples you can use as basis as well as needed documentation.

    Reuse and modify a code example from SDK is the easiest way to manage in my opinion.

    Regards,

    Sebastien.

    Associate
    Dec 23, 2024 9:54 AM UTC

    Hi @Sebastien DENOUAL ,

    What about using BlueNRG-LP as a module with STM32F407, can i use CubeMX as a development IDE in this case?

    if yes, is there any middleware or example project to be used to get start?

    Thanks in advance,

    Regards,

    Sebastien DENOUAL
    ST Employee
    Jan 3, 2025 2:05 PM UTC

    Hi @AhmedHarb96 ,

    Let me share one important update since our initial update 2y ago.

    BlueNRG-LP and BlueNRG-LPS line have benn rebranded as STM32WB06/07 and STM32WB05 respectively.

    The STM32WB0 family's is fully supported by the STM32Cube ecosystem (including CubeMX)

     

    It might answer your initial point.

     

    Regards,

    Seb