Skip to main content
daithi62
Associate II
Oct 19, 2017 4:24 PM UTC
Question

Comms between 2 x IDW01M1 boards

Posted on October 19, 2017 at 18:24

Hi,

I am working on the IDW01M1 wifi module. To-date I have been able to connect 2 of these modules to a common server and send commands between them via the server. I am now trying to connect directly between the modules without the need for the server. I have been able to create an adhoc network but I am unsure about how to setup the boards as both clients and servers. I have searched for any setup information for communicating between 2 IDW01M1 boards and have not been successful.

Could anybody point me in the right direction as to how I could get communications going directly between 2 boards.

Regards,

COD

#wifi-spwf01sa #idw01m1
    This topic has been closed for replies.

    1 reply

    daithi62
    daithi62Author
    Associate II
    Oct 23, 2017 4:10 PM UTC
    Posted on October 23, 2017 at 18:10

    I have one board setup as a server and the other board setup as a client and when I try to connect I am receiving 'WIND: 74 Rejected found Network'. I was able to connect to my android phone earlier using this method.

    # Status & Statistics:

    # version = 170111-665d284-SPWF01S

    # reset_reason = 2

    # conf_flag = 5

    # system_uptime = 149

    # system_sleeptime = 0

    # gpio_enable = 0

    # captiveportal = 0

    # wifi_state = 5

    # wifi_bssid = 00:00:00:00:00:00

    # wifi_aid = 0

    # wifi_channelnum = 0

    # wifi_sup_rate_mask = 0x003FFFCF

    # wifi_bas_rate_mask = 0x0000000F

    # wifi_chan_activity2 = 0x00001FFF

    # wifi_max_tx_power = 12

    # wifi_gf_mode = 0

    # wifi_regccountry DE

    # wifi_dtim_period = 1

    # wifi_sleeping = 0

    # wifi_num_assoc = 0

    # ip_ipaddr = 0.0.0.0

    # ip_netmask = 0.0.0.0

    # ip_gw = 0.0.0.0

    # ip_dns = 0.0.0.0

    # ip_dns2 = 0.0.0.0

    # ip_sock_open = 0

    # ip_sockd_port = 0

    # free_heap =20024

    # min_heap = 19784

    # current_time = 606

    =================================================

    # Dumping All Configuration Keys:

    # nv_manuf = STM

    # nv_model = SPWF01SA11

    # nv_serial = value

    # nv_wifi_macaddr = 00:80:E1:B9:77:BD

    # etf_mode = 0

    # blink_led = 0

    # wind_off_low = 0x00000000

    # wind_off_medium = 0x00000000

    # wind_off_high = 0x00000000

    # user_desc = anonymous

    # escape_seq = at+s.

    # localecho1 = 0

    # console1_speed = 115200

    # console1_hwfc = 1

    # console1_enabled = 1

    # console1_delimiter = 0x000000CC

    # onsole1_errs = 1

    # sleep_enabled = 0

    # standby_enabled = 0

    # standby_time = 10

    # wifi_tx_msdu_lifetime = 0

    # wifi_rx_msdu_lifetime = 0

    # wifi_operational_mode = 0x00000011

    # wifi_beacon_wakeup = 1

    # wifi_beacon_interval== 100

    wifi_listen_interval = 0

    # wifi_rts_threshold = 3000

    # wifi_ssid = 43:54:41:43:53:5F:41:64:68:6F:63:5F:45:72:6E:65:73:74:00:00:00:00

    :00:00:00:00:00:00:00:00:00:00

    # wifi_ssid_len = 18

    # wifi_txfail_thresh = 5

    # wifi_dtim_period =1

    # wifi_add_tim_ie = 1

    # wifi_ht_mode = 0

    # wifi_channelnum = 1

    # wifi_opr_rate_mask = 0x00003FCF

    # wifi_bas_rate_mask = 0x0000000F

    # wifi_mode = 1

    # wifi_region = 1

    # wifi_auth_type = 0

    # wifi_atim_window = 0

    # wifi_powersave= 0

    # wifi_tx_power = 12

    # wifi_rssi_thresh = 0

    # wifi_rssi_hyst = 0

    # wifi_ap_idle_timeout = 120

    # wifi_beacon_loss_thresh = 10

    # wifi_priv_mode = 2

    # wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wiii_wep_eys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_wep_key_lens = 00:00:00:00

    wifi_ep_default_key = 0

    # wifi_wpa_psk_raw = 99:26:E4:84:73:1C:58:8E:1D:17:B5:08:DF:E8:B2:92:E2:64:12:4

    3:9D:17:37:E9:57:68:21:15:C8:7A:E3:DD

    # wifi_wpa_psk_text = T1tpfctaahn

    # ip_use_dhcp = 1

    # ip_use_httpd = 1

    # ip_mtu = 1500

    # ip_hostame = iwm-B9-77-BD

    # ip_apdomainname = captiveportal.net

    # ip_apredirect = firstset.html

    # ip_ipaddr = 192.168.0.123

    # ip_netmask = 255.255.255.0

    # ip_gw = 192.168.0.1

    # ip_dns = 192.168.0.1

    # ip_http_get_recv_timeout = 3000

    # ip_ait_timeout = 12000

    # ip_dhcp_timeout = 20

    # ip_sockd_timeout = 250

    # ip_dhcp_lease_time = 120

    # ip_dns_mode = 0

    # ip_use_cgis = 0x0000000F

    # ip_use_ssis = 0x0000000F

    # ip_use_decoder = 0x00000000

    # ip_block_pings = 0

    Thanks,

    cod