Skip to main content
MDaya.2
Associate II
Sep 12, 2023 10:13 AM UTC
Question

Capacitive SENSOR with STM32

Hello to everyone. I am trying to see the data via I2C with the capacitive sensor (FDC2214-Q1),

but I see the values I have assigned as 0 in live experiment.

I'm sure about the hardware part. I would be happy if you help.

 

 

/* Private define ------------------------------------------------------------*/

/* USER CODE BEGIN PD */

#define FDC2214_I2C_ADDR_0 0x2A // Address is 0x2A (default) if 0x2B (high) //

#define FDC2214_I2C_ADDR_1 0x2B

#define FDC2214_DEVICE_ID 0x7F

#define FDC2214_DATA_CH0_LSB 0x01

#define FDC2214_DRIVE_CH0 0x1E

#define FDC2214_DATA_CH0_MSB 0x00

#define FDC2214_DATA_CH0 0x00

static char value_str[10];

uint32_t value = 0;

uint16_t lsb_buffer = 0;

uint16_t msb_buffer = 0;

uint8_t *lsb_buffer_ptr = (uint8_t *)&lsb_buffer;

uint8_t *msb_buffer_ptr = (uint8_t *)&msb_buffer;

 

 

//HAL_StatusTypeDef HAL_I2C_Mem_Read(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint16_t MemAddress, uint16_t MemAddSize, uint8_t *pData, uint16_t Size, uint32_t Timeout)

HAL_I2C_Mem_Read(&hi2c1, FDC2214_I2C_ADDR_0, FDC2214_DATA_CH0, 1, msb_buffer_ptr, 1, HAL_MAX_DELAY);

HAL_I2C_Mem_Read(&hi2c1, FDC2214_I2C_ADDR_0, FDC2214_DATA_CH0_LSB, 1, lsb_buffer_ptr, 1, HAL_MAX_DELAY);

 

value = value | lsb_buffer; // 0000 0000 | 0000 XXXX = 0000 XXXX VALUE lsb'sini doldurdum.

msb_buffer = msb_buffer & 0x0FFF; // msb_buffer'ın ilk 4 bitini 0 ladım. Datasheet'e göre 12 biti lazım. // Gelen ilk degeri 0 dışında bir şey görüyorum

value = (msb_buffer << 12) | value; // msb_buffer'ı value'nun MSB kısmına kaydırdım ve orlayarak MSB kısmını doldurdum. 0000 XXXX | 0XXX 0000 = 0XXX XXXX

 

sprintf(value_str, "%ld", value);

 

// USART üzerinden veriyi gönder

HAL_UART_Transmit(&huart1, (uint8_t *) value_str, sizeof(value_str), HAL_MAX_DELAY);

 

 

 

 

while (1)

 

 

This topic has been closed for replies.

2 replies

Issamos
Super User
Sep 12, 2023 10:57 AM UTC

Hello @MDaya.2 

I suggest you to double check your device id, your i2c address and the validity of the data provided by your sensor. 

Else I suggest you to debug your code to get the source of error.

Best regards.

II

TDK
Sep 12, 2023 1:08 PM UTC

HAL expects a left-shifted address, so 0x54 or 0x56 for this chip.

Always use HAL_I2C_IsDeviceReady to verify the chip is responding before trying other I2C functions.

"If you feel a post has answered your question, please click ""Accept as Solution""."