Visitor II
Jan 18, 2021 8:40 AM UTC
Question
Cannot connect to BNRG2A1 using normal HCI commands (in Zephyr RTOS)
- 3 replies
- 2002 views
I am not able to establish a BLE connection between the Zephyr RTOS and any other device I have (phone + laptop).
My setup is as follows
- a NUCLEO-L4R5ZI board with a X-NUCLEO-BNRG2A1 shield, powered by the ST-Link over USB from my laptop
- a Digilent Analog Discovery 2 connected to the SPI, CS, and IRQ pins
- Zephyr RTOS 2.4.99 extended with support for the X-NUCLEO-BNRG2A1 shield
I have attached debug log from the nRF Connect Android App (Log 2021-01-14 110432) and a heavily annotated log of the SPI communication between board and shield (sib-connect3)
I was able to port the SensorDemo_BleSensor-App to this board and it is working. Unfortunately it only uses Vendor Specific commands, so it does not help me in analyzing what, if anything, I'm doing wrong...
Your help would be greatly appreciated.
Kind regards,
Wim Yedema