Skip to main content
Visitor II
Mar 5, 2026 12:05 AM UTC
Solved

Can't talk to EVAL-STPM33

I have eval kit EVALSTPM33 from Digikey. When I plug it into my PC USB port, I see a red LED near the USB port, and in the Windows device manager it shows up as com port #6. If I connect to that com port and try to read a register in software from https://www.st.com/en/embedded-software/stsw-stpm001.html, I get an error. After 10 seconds or so the red LED goes out. I do not have anything connected besides the USB port. 

 

Stpm33CommsIssue.jpg

STPM33evalPhoto.jpg

 

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Mar 5, 2026 8:02 AM UTC

Welcome @marc3141, to the community!

Had you ever read UM1748, in particular, section 2.3.2 for commissioning?

In your photo, you can see that you have correctly set SW1 (UART) and J4 (EN), but the STPM33 is not supplied with 3.3V because nothing is connected to J7 (the green 3V3 connector).

Additionally, you should select the correct target in the GUI: in your screenshot, you can see the STPM34, even though you have an STPM33.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Mar 5, 2026 8:02 AM UTC

Welcome @marc3141, to the community!

Had you ever read UM1748, in particular, section 2.3.2 for commissioning?

In your photo, you can see that you have correctly set SW1 (UART) and J4 (EN), but the STPM33 is not supplied with 3.3V because nothing is connected to J7 (the green 3V3 connector).

Additionally, you should select the correct target in the GUI: in your screenshot, you can see the STPM34, even though you have an STPM33.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.