Skip to main content
raphael declercq
Associate II
Apr 27, 2017 8:53 AM UTC
Question

Can I make a beacon advertising and a connectable advertising at the same time?

Posted on April 27, 2017 at 10:53

Hi,

I am working on a x-nucleo-IDB05A1 together with a nucleo-L073.

I would need to advertise Eddystone/iBeacon datas and be connectable at the same time.

My problem is that I can emit beacon data but when I put the device into connectable mode, the beacon stops.

I would need a solution that allows me to emit beacon data and be connectable at the same time.

Does someone knows (if such a thing is possible), how to achieve it?

Thanks in advance,

Raphael

#ble #beacon
This topic has been closed for replies.

4 replies

marchese.graziella
Visitor II
May 5, 2017 8:27 AM UTC
Posted on May 05, 2017 at 10:27

Dear Customer,

to understand how to set a Beacon device, you can see the script BLE_Beacon.py that you can find inside the installation package of BlueNRG but using this script you put a device in discoverable mode but not connectable.

Instead, If you want that the beacon device connectable, you have to modify the command

ACI_GAP_SET_DISCOVERABLE setting the Advertising_Type to 0x00 instead of 0x03

 N.B.: Advertising type Values:

- 0x00: ADV_IND (Connectable undirected advertising)

- 0x01: ADV_DIRECT_IND (Connectable directed advertising)

- 0x02: ADV_SCAN_IND (Scannable undirected advertising)

- 0x03: ADV_NONCONN_IND (Non connectable undirected advertising

Regards

Andrew Neil
Super User
Nov 9, 2017 12:49 PM UTC
Posted on November 09, 2017 at 12:49

Old topic but, for some reason, appeared at the top of the list.

Marchese.Graziella wrote:

Instead, If you want that the beacon device connectable...

But that wasn't the question!

The question was how to do

both

- at the same time.
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
marchese.graziella
Visitor II
Nov 30, 2017 12:03 PM UTC
Posted on November 30, 2017 at 13:03

Dear customer,

you cannot set contemporarly a device in Advertising in not connectable mode and in connectable mode. The state machine of the device permits only one state of advertising.

For example, you set the device in advertising in with Advertising Type = 0x00 ADV_IND (Connectable undirected advertising) in order to be a beacon device connectable, after a connection the beacon device stops (because the device is not more in advertings) but now you can put again the device in advertising (connectable or not connectable mode) in order to be again a beacon device.

Regards,

Graziella
Andrew Neil
Super User
Nov 30, 2017 1:11 PM UTC
Posted on November 30, 2017 at 13:11

I guess you could have the device alternate between advertising 

in not connectable mode, and

advertising 

in connectable mode ... ?
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.